Technical FAQs

Ask a Question

What are the limitations of the FactoryCast HMI 'PLC' Service?

'The maximum number of PLC services for a Quantum NWM module is 1.
And the maximum number of PLC services for a Premium WMY module is 5.
With both modules the maximum number of FactoryCast variables is limited to 1000 for all PLC services.

Additionally, The maximum number of all services for a Quantum NWM module is 6 and the maximum number of all services for a Premium WMY module is 7.


Legacy KB System (APS) Data: RESL180104 V1.0, Originally authored by DaSo on 10/17/2006, Last Edited by DaSo on 10/17/2006
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?