Technical FAQs

Ask a Question

Where to find the gsd configuration file for profibus DP ? (VJD V4.4 - XBTGT)

You can find this .gsd file in the CD 2 of Vijeo-Designer V4.4.
This file is located in the repertory "fieldbus".
You can also find it below :

TELE08DF.gsd


Legacy KB System (APS) Data: RESL180076 V1.0, Originally authored by on , Last Edited by FaMe on 10/16/2006
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?