Technical FAQs

Ask a Question

Is the Twido PLC Class 1, Division 2, certified?

Yes it is. Although not well documented the Twido is suitable for use in Class 1, Division 2, Groups A,B,C,D, or non hazardous locations only.

Was this helpful?
What can we do to improve the information ?