Technical FAQs

Ask a Question

174CEV20040 Ethernet To Modbus Plus Bridge Dimensional Drawing

Goals and Symptoms

The user manual for the 174CEV20040 Modbus Plus to Ethernet Bridge does not have any dimensional
drawings. The goal is to provide the dimensional drawing for the 174CEV20040.

Facts and Changes

174CEV20040 Ethernet To Modbus Plus Bridge

Causes and Fixes

 

  • The following drawing is the FRONT view of the 174CEV20040



The following drawing is the REAR view of the 174CEV20040:



The following drawing is the RIGHT SIDE view of the 174CEV20040:





The following drawing is the TOP view of the 174CEV20040:

Legacy KB System (APS) Data: RESL179915 V1.0, Originally authored by AlCh on 09/28/2006, Last Edited by AlCh on 09/28/2006
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?