Technical FAQs

Ask a Question

Sample of a subroutine using Twidosoft.

Goals and Symptoms
Simple application showing a subroutine using Twidosoft.
Causes and Fixes
Below is the subroutine in ladder and also in list.

Note: The Twido zip file was created in Twidosoft version 3.5 and will not open in any version less than 3.5.




Attachments
(Removed File URL: 179698_C8D2/subroutine.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/9198b6ee1145d473c12579d60011605b/fl_block_5/0.132E?OpenElement&FieldElemFormat=gif)

Legacy KB System (APS) Data: RESL179698 V3.0, Originally authored by DiSa on 09/12/2006, Last Edited by BrWa on 04/04/2012
Related ranges: Twido Soft
Was this helpful?
What can we do to improve the information ?