Technical FAQs

Ask a Question

What do the Memory Protect slide switch settings signify in the 140CPU31110?

Mem Prt Off - allows run/stop CPU and application changes.
Not Used - should not be used as it can lead to undefined operation. Produces "Error while trying to run the project;
mode cannot be changed (ex: an I/O forces the PLC to STOP)" when the user tries to run/stop CPU or
modifiy application.
Mem Prt On - prohibits run/stop CPU or modification of applications.


Legacy KB System (APS) Data: RESL179435 V1.0, Originally authored by DaSo on 08/29/2006, Last Edited by DaSo on 08/29/2006
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?