Technical FAQs

Ask a Question

VJD V4.4 WebGate in XBTGT - CFcard If after downloading your project you get this error : "You can't download WebGate function, second drive is missing"

Goals and Symptoms

VJD V4.4 WebGate in XBTGT panels.
If after downloading your project you get an error :
"You can't download WebGate function, second drive is missing".
Question: Can I use Web Gate in XBTGT panels without CF cards?

Facts and Changes

VJD V4.4 web gate XBTGT cfcard second drive

Causes and Fixes

In VJD V4.4, you need to have a CFcard in the terminal when you want to use the Web Gate functionality with a XBTGT terminal.
This is mandatory because the CFcard is used to create the temporary html files.


Legacy KB System (APS) Data: RESL179275 V1.0, Originally authored by on , Last Edited by on
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?