Technical FAQs

Ask a Question

XBTN front face drawings

Goals and Symptoms

XBTN front face drawings
(dimensions, position and size of the buttons, the screen, ...)

Causes and Fixes

Please see the attached file

Attachments

(Removed File URL: 179050_C522/XBTN-R_front_face.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/5b699be67907ea32c12571b20033e53e/fl_block_5/0.1342?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL179050 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT N, R
Was this helpful?
What can we do to improve the information ?