Technical FAQs

Ask a Question

What are the references and the dimensions of the XBT ZG protective sheets ?

Goals and Symptoms

What are the references and the dimensions of the XBT ZG protective sheets ?

Causes and Fixes

TERMINAL REFERENCE SIZE (in mm)
************************************************************************
XBTGT1100 XBTZG61 126X99.9
XBTGT1130
************************************************************************
XBTGT2110 XBTZG62 131.4X159.4
XBTGT2120
XBTGT2130
XBTGT2220
XBTGT2330
************************************************************************
XBTGT4230 XBTZG64 166X210
XBTGT4330
XBTGT4340
************************************************************************
XBTGT5330 XBTZG65 205X255
XBTGT5340
************************************************************************
XBTGT5230 XBTZG66 231X298
XBTGT6330
XBTGT6340
************************************************************************
XBTGT7340 MPCYK50SPAKIT 236.7X312.7


Legacy KB System (APS) Data: RESL178994 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?