Technical FAQs

Ask a Question

VJL V2.6 : starting VijeoLook, an error "Unable to create ActiveBar Control" appears

Goals and Symptoms

VJL V2.6 : starting VijeoLook, an error "Unable to create ActiveBar Control" appears

Facts and Changes

VijeoLook 2.6 Windows XP unable create active bar control activebar

Causes and Fixes

Some other software may have corrupted your Vijeo Look installation.
Please follow the below procedure :
1- Transfer your authorisation to another PC (using a removable media such as a USB key).
For this, you should use the Registration tool.
2- On your actual computer, uninstall VijeoLook and its components.
Then reinstall VijeoLook and its associated components (so that we'll be sure that the VijeoLook install is clean).
3- Transfer back your authorisation to your actual PC.
Then all should work correctly.


Legacy KB System (APS) Data: RESL178916 V1.0, Originally authored by on , Last Edited by on
Related ranges: Vijeo Look
Was this helpful?
What can we do to improve the information ?