Technical FAQs

Ask a Question

AutoCad Drawing for the Quantum '140 ACI 04000' Module

Goals and Symptoms

Provide an AutoCad drawing on the 'Quantum 140 ACI 04000' module for the ProWORX 32 IO Drawing Generator.

Facts and Changes

The AutoCad drawing for the 'Quantum 140 ACI 04000' module is missing in ProWORX 32 version 2.0B.

Causes and Fixes

Download and extract the files into the C:\ProWORX\32\Drawings folder.
The attached zip file contains two AutoCad drawings with the same file name located in two different folders (Jic and Process).

  • The drawing found in the 'Jic' folder shows the IO card termination.
  • The drawing found in the 'Process' folder shows the IO card and external field wiring termination.

Attachments

(Removed File URL: 178464_C166/ACI040-00.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/9cbf4e8b4b3c9544c125719500838502/fl_block_5/0.612?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL178464 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?