Technical FAQs

Ask a Question

How many ATV31 Altivar Drives can be put on any of the Advantys NIM's with the CANopen extension module STBXBE2100?

Goals and Symptoms
To determine what the maximum number of ATV31 Altivar Drives that can be put on any of the Advantys NIM's with the CANopen STBXBE2100 extension module.
Causes and Fixes
This is the maximum possible ATV31 drives which will be dependant on the Master's features. ( size of cyclic data per slave and total size of cyclic
data.


Legacy KB System (APS) Data: RESL177889 V3.0, Originally authored by DiSa on 09/21/2009, Last Edited by BrWa on 10/19/2012
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?