Technical FAQs

Ask a Question

VJL V2.6 - Unable to enter standby or hibernate modes - Blue screen reboots

Goals and Symptoms

After installing Vijeo Look 2.6 with the option allow lock out Alt-Tab & other keyboard shortcuts I was unable to enter standby or hibernate modes.
I also experienced blue screen reboots with internal power error messages.

Causes and Fixes

Some web research turned up this tip, http://support.microsoft.com/?kbid=314118.

Uninstalling Vijeo Look & then reinstalling it without the keyboard shortcut lockout solved my problem.

Was this helpful?
What can we do to improve the information ?