Technical FAQs

Ask a Question

Converting a Modsoft program that contains loadables does not convert the IO map.

Goals and Symptoms

Converting a Modsoft program that contains loadables to a 'Proworx 32'. project does not convert
the IO map.

Facts and Changes

'ProWorx 32' version 2.1

Causes and Fixes

Converting a Modsoft program that contains loadables to a 'Proworx 32'. project does not convert
the IO map.

To resolve the issue:
1.) Remove the loadable first,
2.) Convert the Modsoft program to a 'ProWORX 32' project.
3.) Add the loadable back into the 'ProWORX 32 ' project.
4.) Save the changes.


Legacy KB System (APS) Data: RESL177699 V1.0, Originally authored by AlCh on 12/16/2010, Last Edited by AlCh on 12/16/2010
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?