Technical FAQs

Ask a Question

VijeoLook V2.6 : during the installation, error "1603" and then another error "Missing MSDN 2000". How to solve it ?

Goals and Symptoms

VijeoLook V2.6 : during the installation, error "1603" and then another error "Missing MSDN 2000". How to solve it ?

Causes and Fixes

During the installation of VijeoLook, if you have a problem with MSDN 2000 (error 1603), then you have to check the Status and the Startup type of those 2 Services "Server" and "Computer Browser" (Control Panel \Administrative Tools \ Services).
They must be started in automatic :
---------------------------------------------------------------------------------------
// Name // Status // Startup Type //
---------------------------------------------------------------------------------------
// Computer Browser // Started // Automatic //
// Server // Started // Automatic //


Legacy KB System (APS) Data: RESL177610 V1.0, Originally authored by on , Last Edited by on
Related ranges: Vijeo Look
Was this helpful?
What can we do to improve the information ?