Technical FAQs

Ask a Question

How to upgrade Vijeo designer V4.3 for XBTGT terminals 7.5"--15" ? Because these targets are not reachable in VJD.

Goals and Symptoms

How to upgrade Vijeo designer V4.3 for XBTGT terminals 7.5"--15" ? Because these targets are not reachable in VJD.

Causes and Fixes

The product leader had decided to lock XBTGT targets 7.5" to 15" because at VJD V4.3 launching, these targets were not available.

But now these targets are available (April 2006), please follow the below procedure to upgrade VJD V4.3 and unlock the XBTGT targets :

1- Authorize VJD V4.3 (to do this, enter VJD V4.3, then click on "Help/About" and select "Authorize". Then follow the information)

2- Upgrade VJD V4.3 and unlock the XBTGT targets you want.
(to do this, enter VJD V4.3, then click on "Help/About" and select "Upgrade".
Then, enter the below codes in order to unlock the XBTGT targets you want.

CODES TO UPGRADE VJD V4.3 AND UNLOCK XBTGT TARGETS :
VJDUPG4XXV43M : unlock GT4xxx targets
VJDUPG5XXV43M : unlock GT5xxx targets
VJDUPG5XXV43M : unlock GT6xxx targets
VJDUPG7XXV43M : unlock GT7xxx targets

3- For your information, these codes are provided with each XBTGT (included in the box). So when a customer receives a XBTGT terminal, he has these codes.


Legacy KB System (APS) Data: RESL177504 V1.0, Originally authored by on , Last Edited by on
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?