Technical FAQs

Ask a Question

What is the depth of the 140CPU534 14A including the backplane?

The 140CPU534 14A including the backplane is 4.34 inches deep.


Legacy KB System (APS) Data: RESL177348 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?