Technical FAQs

Ask a Question

MTBF and Lifetime of the XBTGT/GK range

Goals and Symptoms

What are the MTBF of the XBTGT & XBTGK?

Causes and Fixes


XBTGT2330:
Lifetime: 50000 hours
Mean Time Between Failures : 12418 hours
... (see attached files for all details)
XBTGT5330:
Lifetime: 50000 hours
Mean Time Between Failures :7644 hours


XBTGK2120:
Lifetime: 50000 hours
Mean Time Between Failures : 13058 hours
XBTGK2330:
Lifetime: 50000 hours
Mean Time Between Failures :8673 hours
XBTGK5330:
Lifetime: 50000 hours
Mean Time Between Failures : 6031 hours
(see attached files for all details)

Attachments

(Removed File URL: 177318_B4E6/MTBF_all_xbtgt.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f627976801cfe634c12574560052adbb/fl_block_5/0.1338?OpenElement&FieldElemFormat=gif)(Removed File URL: 177318_B4E6/XBTGK.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f627976801cfe634c12574560052adbb/fl_block_5/0.20B6?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL177318 V2.0, Originally authored by JaOu on 05/27/2008, Last Edited by DaBr on 05/27/2008
Related ranges: Magelis XBT GK, Magelis XBT GT
Was this helpful?
What can we do to improve the information ?