Technical FAQs

Ask a Question

Why is the HSBY Loadable for the 984-68X/78X not included with my Proworx 32 Programming Software?

The HSBY Loadable for the 984-68X/78X is not included with the Proworx 32 Programming Software because it is included when purchasing the Hot Standby Kit (Part# AS-911K-806/812/830). The software loadable is no longer available to ordser.
The HSBY Loadable is attached to prevent any delays in getting this Loadable.

Hsby_8v2.zip


Legacy KB System (APS) Data: RESL1772 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?