Technical FAQs

Ask a Question

How to print a Modsoft program to a pdf file

Goals and Symptoms

How to print a Modsoft program to a pdf file

Facts and Changes

All versions of Modsoft

Causes and Fixes

The following procedure can be used to print a Modsoft program to a pdf file,

1.) Install a pdf printer (you can get one from http://www.fineprint.com/support/pdffactory/ )
2.) Start Modsoft and select the Tools\Print
3.) Select th program to be printed.
4. Click on 'Printer'
5.) Select Flat File (8.5x11) as the printer setting in Modsoft.
and hit the ENTER key.
6.) Type in a filename for the printout (i.e., Modsoft.out).
7.) Click on 'Start and select 'Full Print to print the file Modsoft.out.
8.) Open Notepad.
9.) Using Notepad, locate and open the 'Modsoft.out' file.
10.) Click on File\Print in Notepad
11.) Select the installed pdf printer (i.e., pdfFactory 2).
12.) Wait for the conversion to finish and save the pdf file.

Was this helpful?
What can we do to improve the information ?