Technical FAQs

Ask a Question

ProWORX 32 Appears to be solving some skipped networks when the SKP block is inserted in a populated network

Goals and Symptoms


ProWORX 32 Appears to be solving some skipped networks when the SKP block is inserted in between logic
within the middle of a populated network

Facts and Changes

ProWORX 32 version 2.0

Causes and Fixes

If a SKP block is inserted in between logic within a populated network, it is possible to see power flow still occurring
in the logic on one of the networks that are supposed to be skipped.

Further examination of the registers associated with the logic within the network will in fact show that the
network has been skipped. In addition, the comment field located in the lower right corner of the Logic window
will display the comment 'Netwrok skipped'.

The problem is related to the display update.for the Logic window when the SKP block is used with logic in the same
network.

As a workaround, the SKP block should be inserted in a network that does not contain other logic.


Legacy KB System (APS) Data: RESL176893 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?