Technical FAQs

Ask a Question

Which PLC types support the NBIT instruction in the ProWORX programming software?

The NBIT (Normal Bit) instruction is standard in all the Quantum series PLCs and Compact 32-bit controllers (E984-258/265/275/285).


Legacy KB System (APS) Data: RESL176868 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?