Technical FAQs

Ask a Question

AIDAIG XL : IMPORT FILES MANUALLY

Goals and Symptoms

GOALS : Manage to import manually recordings stored into the AIDIAG Premium XL module
SYMPTOMS : Import on a PC files stored into the module memory, purge module, strategy out of automatic download

Causes and Fixes

FIX : Follow procedure described in the PDF file

Attachments

(Removed File URL: 176591_B206/gbn_4_-_recordings_manual_imports.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7c29e543bbebd739c125713e004ed5c4/fl_block_5/0.578?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176591 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?