Technical FAQs

Ask a Question

AIDIAG XL : DATA STORAGE FOLDER MANAGEMENT

Goals and Symptoms

GOALS : The AIDIAG Premium Black Box manager needs a file dedicated to the storage of its data and recordings imported from the AIDIAG Premium XL Black Box. Then , during its first execution, it is imperative to define the storage folder, see procedure creation of the Storage folder into the PDF.
SYMPTOMS : First use of AIDIAG Premium Black Box manager, or during folder changes

Causes and Fixes

FIX : See procedure on the PDF file

Attachments

(Removed File URL: 176588_B1FA/gbn_1_-_Data_Storage_folder_managment.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/81e3524a095d499ac125713e004ed4e2/fl_block_5/0.580?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176588 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?