Technical FAQs

Ask a Question

AIDMAP II : ADD A MARKER

Goals and Symptoms

GOALS : A time stamp allows to do the first level of chronograms analyze, it allows the user to: Display variables synchronism, Measure the time between two stamps, Specify a particular event.

Causes and Fixes

FIX : Check the PDF file to know how to add markers ( time stamp)

Attachments

(Removed File URL: 176567_B1BE/aidmap_13_Add_marker.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/fb79aec81c49399bc125713c00053182/fl_block_5/0.55E?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176567 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?