Technical FAQs

Ask a Question

AIDMAP II : CONVERT A BOOLEAN TO AN INTEGER

Goals and Symptoms

GOALS : Allows creation of integer variables from Boolean ones. Allows to have a proper view of the signal shape
SYMPTOMES : Boolean variables represent an integer value, this system allows you to convert them and get an image of the variable evolution in the time

Causes and Fixes

FIX : Use AIDMAP II function, follow directions of PDF file

Attachments

(Removed File URL: 176566_B1BA/aidmap_10_convert_booleen_to_integer.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f90fae8762cc6af4c125713c00053169/fl_block_5/0.57E?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176566 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?