Technical FAQs

Ask a Question

AIDMAP II : VARIABLES SORTING

Goals and Symptoms

GOALS : Sort module variables list in a pre defined order
SYMPTOMS : The number of variables available may make the display unclear, therfore you can apply a pre defined automatic sorting based on different elements

Causes and Fixes

FIX : Follow the sorting direction on the PDF file

Attachments

(Removed File URL: 176564_B1B2/aidmap_7_variables_sorting.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/6b719b878024a228c125713c000530fe/fl_block_5/0.56A?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176564 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?