Technical FAQs

Ask a Question

AIDMAP II : CONVERT INTEGER TO BOOLEAN DATA

Goals and Symptoms

GOAL : Create Boolean variable from an integer one, allow to customize the analyze
SYMPTOM : Will to get more precision from the API values by converting an Integer signal into Boolean values

Causes and Fixes

FIX : Use AIDMAP II's integrated function, following the pdf file explaination

Attachments

(Removed File URL: 176563_B1AE/aidmap_11_convert_integer_to_boolean.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/9f71f1d5c05f0920c125713c000530d7/fl_block_5/0.57E?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176563 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?