Technical FAQs

Ask a Question

AIDMAP II : CREER DES VARIABLES CALCULEES

Goals and Symptoms

GOALS : Enable the combination of variables, to highlight a time, a movement, or a particular situation.
SYMPTOMS : Need to create variables relating to your process analyze, these variables rely on calculated or logical functions allowing the user to create his own formula

Causes and Fixes

FIX : AIDMAP II proposes a wide range of calculating functions , easy to use, which behave like usual values

Attachments

(Removed File URL: 176562_B1AA/aidmap_12_Add_calculated_variables.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/305ca3b0a4e75f59c125713c000530d3/fl_block_5/0.57A?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176562 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?