Technical FAQs

Ask a Question

AIDMAP II : IMPORT / EXPORT BETWEEN AIDMAP FILES

Goals and Symptoms

GOALS :It is possible to Import or Export an AIDMAP II configuration on a totally strict manner. This tool has, as direct application, a complement to AIDIAG Premium Black Box function to allow fast application of a configuration on existing variables.
SYMPTOMS : Once you made your analyze on one acquisition file, you want to apply it to others files you've got from this process. Therfore, you can use this function to Export or Import the right configuration to your file, it will organize by itself all variables and folders

Causes and Fixes

FIX : USe the Import / Export function as explained into the PDF file

Attachments

(Removed File URL: 176561_B1A6/aidmap_15_Import-export_between_aidmaP_II_files.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/960dd9cd60a695e8c125713c00053092/fl_block_5/0.594?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176561 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?