Technical FAQs

Ask a Question

AIDMAP II : TYPE OF VARIABLES AVAILABLE

Goals and Symptoms

GOALS :Allows to quickly know variables origin ( PLC variables, AIDMAP II variables) or the type of variables (Boolean, Integer…).
SYMPTOMS : Need to understand quickly all variables available on a system

Causes and Fixes

CAUSE : Many variables available on a process, different types and object
FIX : See decription on PDF file

Attachments

(Removed File URL: 176560_B1A2/aidmap_8_type_of_variables.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/9ec5f05fb2b24756c125713c00053084/fl_block_5/0.56A?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176560 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?