Technical FAQs

Ask a Question

AIDMAP II : ADD SYMBOLS AND COMMENTS TO VARIABLES

Goals and Symptoms

GOAL : On a manual or automatic way, symbols and comments are associable to each OPC or AIDMAP II variables.
SYMPTOMS : Number of variables, symbols and comments allow the user to implement any information on the valuable variables ( like a name, movement description,....)

Causes and Fixes

CAUSE : Need to customize the application file to a process
FIX : Get solutions from the PDF file

Attachments

(Removed File URL: 176559_B19E/aidmap_9_Add_symbols_and_comments.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/49528cf027f36ff1c125713c0005307d/fl_block_5/0.578?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176559 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?