Technical FAQs

Ask a Question

AIDMAP II : INCREASE DISPLAY RESOLUTION

Goals and Symptoms

GOALS : Have a better view of the signals to ease analyze
SYMPTOMS : The resolution is not adapted to the signal length or shape

Causes and Fixes

CAUSES : The resolution scale allows the user to go from a large view of the process to a really detailed view of a signal, up to the millisecond
FIX : Follow method on PDF file

Attachments

(Removed File URL: 176558_B19A/aidmap_6_Increase_the_resolution.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/d0d11465359fa783c125713c00053064/fl_block_5/0.576?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176558 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?