Technical FAQs

Ask a Question

AIDMAP II : EXPORT DATA FROM THE SOFT

Goals and Symptoms

GOALS : Export AIDMAP II data to an other application
SYMPTOMS : Need of using AIDMAP data ( statistics, Time stamping sheet,...) into an other application such as Excell, Word, PPoint,

Causes and Fixes

FIX : Follow method described on PDF file

Attachments

(Removed File URL: 176550_B18A/aidmap_5_Export_data_from_AIDMAP.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/43c03c2cb666e72fc125713b00561072/fl_block_5/0.576?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176550 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?