Technical FAQs

Ask a Question

AIDMAP II : ORGANIZE INFORMATIONS IN MODULE

Goals and Symptoms

GOAL : Organize the data to get a more clear, easy to handle, and attractive application and analyze
SYMPTOM : A lot of data are monitored at the same time, it is necessary to sort the folders and files to have a really clear, customized and easy to handle displaying

Causes and Fixes

CAUSES : 2048 variables recordable on the same file, many useless internal words, need to create your own anlyze folders
FIX : Create folder, , Copy / Paste, move, everything as any Windows based software. See process in Pdf file.

Attachments

(Removed File URL: 176528_B15E/Aidmap_2_organize_informations_in_modules.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/27892196a172560cc125713b00057dbc/fl_block_5/0.588?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176528 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?