Technical FAQs

Ask a Question

AIDMAP II : DEFINE A RECORDING STRATEGY

Goals and Symptoms

GOAL : Define an autorecording parameter to get only the informations needed and let the acquisition work in stand alone
SYMPTOM : Continuous recording, need to schedule the acquisition, and define which variable to monitor in the way to only get valuable data

Causes and Fixes

CAUSES : Continuous recording provide very large files, or you have to stop and run the acquisition every day. Therfore there's a need to create an automatic acquisition , allowing you to define the schedulation of recordings, and define the data valuable for your analyze....
FIX : Follw Pdf file to create your automatic acquisition

Attachments

(Removed File URL: 176527_B15A/aidmap_4_Define_a_recording_strategy.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/290dc04a61b21121c125713b00057db7/fl_block_5/0.57E?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176527 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?