Technical FAQs

Ask a Question

AIDMAP II : STATISTICS PROCESSING

Goals and Symptoms

GOALS : Processing variables statistics available on AIDMAP II : Mnemonic, commentaries, length ( max, min, average, total..) of activity or unactivity, number of activation / unactivation, values, modal, graphics
SYMPTOMS : Device acquiring or file reading, need more detailed information to analyze the signals / process

Causes and Fixes

CAUSE : Need to go further into data anlyzing, need to get some valuable data into process understanding
FIX : Follow the method described hereafter to use the calculated functions

Attachments

(Removed File URL: 176526_B156/aidmap_1_processing_statistics.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/fe4ca2ac88c52139c125713b00057d8a/fl_block_5/0.572?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176526 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?