Technical FAQs

Ask a Question

AIDMAP II : INFORMATION MONITORING VIA AIDIAG

Goals and Symptoms

GOAL : Acquire and monitor data from AIDIAG PREMUM module
SYMPTOM : AIDIAG Module installed, connected to the PC, will to enhance AIDMAP II recording

Causes and Fixes

CAUSES : Need to establish the connection and launch data acquisition from AIDMAP II to AIDIAG PREMIUM
FIX : Use the method explained in the Pdf file

Attachments

(Removed File URL: 176523_B14A/aidmap_0_information_monitoring_via_AIDIAG_-ev0.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/e909f27c0e5630a2c125713b00057d04/fl_block_5/0.594?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176523 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?