Technical FAQs

Ask a Question

AIDIAG : ASSIGN AN IP ADDRESS TO THE MODULE

Goals and Symptoms

GOALS : Enhance the communication between the module and the PC
Symptoms : The IP address of the module doesn't correspond to the network , the PC, or the organization needs

Causes and Fixes

CAUSES : Differences between IP address available or useful and module address
FIX : Assign an IP address to the module by applying a mask on the address

Attachments

(Removed File URL: 176517_B136/aidiag_2_Assign_an_IP_adress-_ev0.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/4fc47aeaf0ae0a16c125713a00633ff8/fl_block_5/0.578?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176517 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?