Technical FAQs

Ask a Question

AIDIAG : SET AN EXTENSION RACK FOR THE MODULE

Goals and Symptoms

GOALS : Use the AIDIAG Module on a different Rack than the PLC's
Symptoms : No slots available on the PLC's Rack, or not enough power supply on it : need to set an extension Rack

Causes and Fixes

The rack was sized before scheduling the module implementation.
Fix : Create a new rack dedicated to the AIDIAG Module, install it, declare it to the PLC

Attachments

(Removed File URL: 176514_B12A/aidiag_1_Add_a_rack_for_AIDIAG_-ev1.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/296f5dba2365a62ac125713a00633f62/fl_block_5/0.57C?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL176514 V1.0, Originally authored by on , Last Edited by on
Related ranges: PROSYST solutions
Was this helpful?
What can we do to improve the information ?