Technical FAQs

Ask a Question

Where on the mains choke for the Lexium high power drive do you connect the shield cable?

Goals and Symptoms

The shield cable is connected to the choke at the ground/shield stud as shown below.

Causes and Fixes

See picture below.



 


Legacy KB System (APS) Data: RESL176440 V1.0, Originally authored by on , Last Edited by on
Related ranges: Lexium 17D
Was this helpful?
What can we do to improve the information ?