Technical FAQs

Ask a Question

What is the heat dissipation on the chokes and filters used with a high power Lexium drive?

The heat dissipation data are:
A) AMOEMC118 - EMC filter appr. 30 W

B) AMOEMC212 - EMC filter appr. 50 W

C) AMOCHK170 - Mains choke appr. 145 W

D) AMOCHK212 - Mains choke appr. 150 W


Legacy KB System (APS) Data: RESL175943 V1.0, Originally authored by on , Last Edited by on
Related ranges: Lexium 17D
Was this helpful?
What can we do to improve the information ?