Technical FAQs

Ask a Question

Problem Viewing STBNIP2212 Ethernet NIM Web Page Applets

Release Notice

The purpose of this Resolution is to inform Advantys users that a problem viewing web page applets from an STBNIP2212 Ethernet NIM has been resolved.

Goals and Symptoms

Web browsers with SUN Java versions 1.5 do not properly display Advantys NIM web page applets. These pages only display a blank gray area but static (text) web pages would display properly

Facts and Changes

Installing SUN Java version of 1.5.0_6 (called update 6) or higher into Windows browsers allows the Advantys web page applets to be viewed properly.

Causes and Fixes

Use this link to download a 16Meg offline file:, OR

  • Run the attached file (, which requires an Internet connection to complee the installation.
Was this helpful?
What can we do to improve the information ?