Technical FAQs

Ask a Question

Is there an EARS Loadable Block for Concept or Unity Pro

Goals and Symptoms

Is there an EARS Loadable Block for Concept or Unity Pro

Causes and Fixes

EARS is an old 984 based loadable that is used in the the plc application to send an ASCII message to a Digiboard device or other HMI. It is only supported on the older 984 based plc's. We have not converted it for use in the Windows based Concept or UNITY Pro software. Currently, there are no plans to convert it.

It has never been tested with the Quantum plc or Concept's 984 ladder logic.


Legacy KB System (APS) Data: RESL175549 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?