Technical FAQs

Ask a Question

List of tested printers - XBTG/XBTGT (Vijeo-Designer V4.3)

A list of the tested printers is available in the online help of Vijeo-Designer V4.3, section "2.4 - Connection Checked Units (printer)".
You can find a printscreen of this section 2.4 in the attached document ("list of printers"). Don't forget that this is not an exhaustive list.

list of printers.zip


Legacy KB System (APS) Data: RESL175450 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?