Technical FAQs

Ask a Question

List of tested Barcode readers - XBTG/XBTGT (Vijeo-Designer V4.3)

A list of the tested Barcode Readers is available in the online help of Vijeo-Designer V4.3, section "2.4 - Connection Checked Units (Bar Code Reader)".
You can find a printscreen of this section 2.4 in the attached document ("list of barcode readers"). Don't forget that this is not an exhaustive list.

list of barcode readers.zip

And just for your information, I have also tested the DataLogic D120 Gryphon series with the CAB-362 cable (RS 232, sub-D9) on XBTG, with VJD V4.3 and it works.


Legacy KB System (APS) Data: RESL175449 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?