Technical FAQs

Ask a Question

How can I correct the Concept error message '1376 - You reached the maximum number of FBInstances allowed in a Section'?

In a ST, FBD, or LD section the limitation is 512 instances of function blocks per section. Once this limit is reached, the user would have to create another section.


Legacy KB System (APS) Data: RESL175064 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?