Technical FAQs

Ask a Question

How do I resolve the "Error 5: Invalid procedure call or argument" when trying to open a workspace file from a networked PC using Advantys configuration software minimum version 2.0?

Goals and Symptoms

To be able to open an Advantys workspace file from a networked PC instead of your local PC.

Facts and Changes

Advantys Configuration software minimum version 2.0

Causes and Fixes

This error can be resolved by using Windows Explorer -> Tools -> Map Network Drive and mapping a drive letter on the local PC to point to a network PC. Then go into the Advantys configuration software and select Settings under the Options menu. Then change the Default file path to the previously mapped drive and projects folder.

Legacy KB System (APS) Data: RESL175003 V4.0, Originally authored by MiRo on 11/15/2007, Last Edited by DaSo on 08/20/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?