Technical FAQs

Ask a Question

How do I set-up HyperTeminal so I can program my AS-B885-002 ASCII/BASIC Module?

The default communication parameters for the AS-B885-002 ASCII/BASIC Module is 1200 baud, 8 data bits, no parity and 1 stop bit. Below are other settings that need to be set:


Legacy KB System (APS) Data: RESL1750 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?