Technical FAQs

Ask a Question

What does the error "Overflow Min <= Value >= Max" mean on my Magelis terminal ?

An operator will get this error when a "Threshold" has been set on the field and the value being entered is outside the threshold.


Legacy KB System (APS) Data: RESL174974 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT F, TXBT F
Was this helpful?
What can we do to improve the information ?